This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recursion in Codec



EVM6446 , dvevm1.20

I compile videnc_copy with debug type (Pkg.attrs.profile = "debug" in package.bld file).  I write a recursion in videnc and compile it, my application will not respond after runing this alg. So I debug videnc in CCS, it does not have any problem. Then I try to comment "Pkg.attrs.profile = "debug""  in package.bld file and then I recompile it, this time my application works. I don't know why codec can not run recursive code in debug mode.

Here is recursive function.

void Transferarray(unsigned short* varray,int icount)
{
    short tmp;
    if(icount < 2)
        return;
    tmp = *(varray+icount-1);
    *(varray+icount-1) = *varray;
    *varray = tmp;
    Transferarray(varray+1,icount-2);
}

 

you can try it in XXXX_XXX_process function, and check whether it can work well in debug mode, thanks.

 

Lorry