This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-C6748: C6748

Part Number: PROCESSOR-SDK-C6748
Other Parts Discussed in Thread: SYSBIOS

Tool/software: TI-RTOS

Hi,

   MMC/SD TATFS examples is generated from OMAP Processor-SDK 4.3. I build a project to debug this example in CCS8.1. Now,there are some problems were encountered during debugging. This problem is printed in CCS console is that  "[C674X_0] ti.sysbios.family.c64p.Hwi: line 189: E_invalidIntNum: Invalid interrupt number: intr# 0", in addition, they UART print "All tests have PASSED 0:>". But when I input some command such as 'ls', 'help', there are not any response to that command. DO you have any suggestions for me to solve those problems.

Best regards

Yuan