This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Transient overshoot/undershoot

Guru 10235 points
Part Number: AM5728

Hello, TI Experts,

 

Our customer sent us a questions about AM5728 datasheet(SPRS953D)

"Table 5-1. Absolute Maximum Rating Over Junction Temperature Range".

 

Question:

Their understanding of "VIO (Transient Overshoot/Undershoot)" is as below;

   - The Note said "valid for up to 20% of the signal period"

   - They use vddshv3 = +3.3V (VDD)

   - Transient Overshoot = +3.96V (= 3.3 + 3.3 x 0.2 )

   - Transient Undershoot = -0.66V (= 0 - 3.3 x 0.2 )

Is this understanding correct?

 

Best regards,