Other Parts Discussed in Thread: OMAP3503, OMAP3530
Hi.
I build WinCE 6.0 image with Silverlight(SYSGEN_XAML_RUNTIME) and DirectDraw(SYSGEN_DDRAW) support.
Image build with flags BSP_XRPLUGIN_DDRAW and SYSGEN_SAMPLEXAMLPERF also.
When i try to start Carousel example, But i have no window appear on the screen, only "XAML ..." on taskbar.
If i build image without BSP_XRPLUGIN_DDRAW flag, all examples starts with window shows, but all examples executes too slowly .
For test purpose i try to play avi-file in TCPMP-player with DirectDraw as Video Driver, and i have the same problem - i see nothing.
Could anybody help me?
OMAP3503, BSP 6.14.01.01