This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSPLink problems with the DM6467

I have managed to get myself confused with regards to dsplink.

I am running on the DM6467 with dvsdk_1_40_00_28, DSPLink 1.50.

I had to change the DSP memory map to fit our application needs, so I cannot use the default map that the examples use.

My application gets the the memory map from the server using the createFromServer function, and that seems to work fine.

Do I need to rebuild dsplinkk.ko in order to match the memory map that the server and application are trying to use?  I thought I needed to, but I am not sure after looking through more documentation.  I get mixed results when I build it... it works with some builds of my app, but not others.