Part Number: TDA2EX17EVM
Tool/software: Linux
Dear Sirs:
We have a TDA2EX17EVM and a UB964 EVM with 4 OV10635 cameras. We use VSDK 03_04_00_00.
The demo in BIOS code for this UB964+10635 in CSI2/CAL demo (usecase mutli-camera==>7: OV10635 & UB964 4CH CSI2 Capture + Display)is perfect that all channels has output from OV10635.
The BIOSs logs shows ISSCAPTURE Link has frames output from it.
However the same demo in Linux version(multi-camera==>a: 4CH CSI2 CAL capture + SgxFrmCpy + DISPLAY - Only HDMI 1080p display supported) is not working at all.
The Linux logs shows nothing in ISSCAPTURE Link.
Both of the testings are setting the source of capture from CHAINS_CAPTURE_SRC_UB964_OV1063X.
The H/W I used to test it is identical, do you have any idea on it?
Regards,
/ckhsu