This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530DCBBA BGA composition

Hello,

Can anyone tell me the following on the OMAP3530DCBBA ,

1. Density of the BGA balls?

 

2. What are the balls made of?

 

3. Specific alloy mixture used?

  • Hello Ken,

    •  the CBB package is a .4mm PGBA for the 515 bottom balls.  The top PoP balls are .5mm pitch and there are 168 balls.
    • The balls are Green (RoHS and no Sb/Br).  this is defined as "Green to mean Pb-Free, and free of Bromine and Antimony based flame retardants (Br and Sb do not exceed 0.1% by weight in bomogeneous material).  for the CBB package they are composed of 98.3%Sn/ 1.2%AG/ 0.5%Cu.