Part Number: AM5718
Tool/software: Linux
Hi
I am using AM5718 processor for a custom board. The two outputs of DSS are LCD1 and LCD2 (both in MIPI DPI). The LCD1 output is routing to a Flatlink Receiver(SN65LVDS 86) and LCD2 output is routing to a Video DAC (ADV7393). The outputs expected from these two ICs are - Flatlink Rx : LVDS output and Video DAC : Analog output(Y/C).
My questions are :
What are the video formats does AM5718 supports as DSS outputs (LCD1,LCD2) ?
I want to generate LVDS output in Progressive scan format and Y/C output in Interlaced scan format.How to get this ?
It will be very helpful if someone provides any idea in order to achieve this.
Does the display supports (1024*768) and (640*480) resolution format ? If yes , is there any specific places where we have to mention this specifications or any other way to get this ?
Thanks and regards
Arpita