Can I find somewhere clarification about values recommended for DM365 Video DAC Configuration (VDAC_CONFIG 0x01C4002C) register? The register (located in System Control Module) contains a number of reserved bits, description of the bits says "any writes must always have a value of 0". Right after the description table, there is recommended value for SD DAC configuration 0x101941DC; if you look into Spectrum DIgital Test codes, you'll find third value. Do the reserved bits have any effect on video DAC work? What are correct values for writing to these reserved fields?