Hi,
I have a question about AM5728 PRU-ICSS.
I understand that PRU can be used as Ether(10/100Base).
AM5728 have PRU0 and PRU1. Each PRU have 2 ether port.
I'm planning to use two ether port of peripheral and one ether port of PRU.
To use only one ether port of PRU, are there any limitation such as only this port of this PRU can be used?
In following TI wiki page, it said as follow:
processors.wiki.ti.com/.../PRU-ICSS_Ethernet Ethernet&tisearch=Search-EN#Single_Port_Mode
/////////////////////////////////////////////////////////////////////////////////////////
On the AM572x IDK the silkscreen says PRU2 ETH0 and PRU2 ETH1 for the supported PRU ports.
/////////////////////////////////////////////////////////////////////////////////////////
Is this means that only PRU2 ETH0 and PRU2 ETH1 can be used in AM572x?
Or is it only related to the IDK board?
best regard,
g.f.