Hi all,
I am using vesa color bar sample program given in PSP drivers of DVSDK of DM648.
I am able to display the VESA color bar pattern on video port 1.
Now i wanted to test this with all the other video ports, basically i want to test all video ports that they are working fine.
But from some where on internet i found that video encoder chip (THS8200) is connected with only port 1, so when ever i use port other than 1 in vesa color bar test program it fails.
I just wanted to know that is it tttrue that i can not use video port other than 1 for this test.
if any body had done this previosly please help me to solve this.
any other information willl also help me.
Regards,
Zuber Saiyed