Part Number: AM5728
Other Parts Discussed in Thread: PMP
Tool/software: Linux
hi
i installed sdk in my desktop pc and connected am5728 evm to pc using debug cable. i connected evm to router where my pc is connected.but not able to boot the evm via minicom. log attached . kindly resolve at the earliest.
U-Boot SPL 2017.01-gc68ed086bd (Mar 26 2018 - 17:06:19)
DRA752-GP ES2.0
Trying to boot from MMC1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2017.01-gc68ed086bd (Mar 26 2018 - 17:06:19 -0400)
CPU : DRA752-GP ES2.0
Model: TI AM572x EVM Rev A3
Board: AM572x EVM REV A.3A
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
reading uEnv.txt
1533 bytes read in 4 ms (374 KiB/s)
Importing environment from mmc0 ...
ethernet@48484000 Waiting for PHY auto negotiation to complete. done
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
DHCP client bound to address 172.16.10.76 (1307 ms)
link up on port 0, speed 100, full duplex
Using ethernet@48484000 device
TFTP from server 172.16.24.25; our IP address is 172.16.10.76; sending through 1
Filename 'zImage-am57xx-evm.bin'.
Load address: 0x82000000
Loading: T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again
link up on port 0, speed 100, full duplex
Using ethernet@48484000 device
TFTP from server 172.16.24.25; our IP address is 172.16.10.76; sending through 1
Filename 'am57xx-evm-reva3-cam-ov10635.dtb'.
Load address: 0x88000000
Loading: T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again
=>