Other Parts Discussed in Thread: AM1808
Hello,
Need Android on Omap-L1x/ Am18x EVm/Hawkbaords.
Thanks!
Best Regards
Feroz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM1808
Hello,
Need Android on Omap-L1x/ Am18x EVm/Hawkbaords.
Thanks!
Best Regards
Feroz
We don't have an official TI DevKit release for AM1808 / OMAP L 138. However, we have already added AM1808 support to Android repository on Rowboat GIT. We will provide detailed instructions on using these on AM1808 EVM by end of this week.
Regards,
Khasim
Hello Khasim,
Can you please share the link for Android port on AM1808 please?
Thanks & Regards
Feroz
The download instructions for Am1808 android devkit are available at http://processors.wiki.ti.com/index.php/TI-AM1808-Android-FroYo-DevKit_UserGuide
Hi Khasim,
I have an AM1808 SOM module based board and I'm trying to port froyo on the that based on the instructions in the link above.
I see a kernel hang. Attaching the log here, I have ensured that the machine numbers match and enabled low level kernel debugging options. Any pointers here?
U-Boot 2009.11 (May 07 2011 - 10:41:02)
I2C: ready
DRAM: 128 MB
NAND: 128 MiB
MMC: davinci: 0
Bad block table found at page 65472, version 0x01
Bad block table found at page 65408, version 0x01
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
U-Boot >
U-Boot > tftp
Using device
TFTP from server 10.0.0.10; our IP address is 10.0.0.11
Filename 'uImage'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#####################################
done
Bytes transferred = 853980 (d07dc hex)
Automatic boot of image at addr 0xC0700000 ...
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.32
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 853916 Bytes = 833.9 kB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux.......................................................... done, booting the kernel.
Make sure that the bootargs for console=ttySx matches your board configuration. No messages from the kernel are seen in your bootlog.
Also make sure you put an initlogo.rle file in the root directory on the SD card you make for the android root fs. Mine would not get past init to the Android GUI without this.
If your kernel is hanging, check to make sure the mem=X setting in your uboot bootargs env var is set correctly. This will most definitely result in nothing after the decompress. its also likely that console=X is not set right...
here is my bootargs setting
bootargs=init=/init console=ttyS2,115200n8 ip=off rw root=/dev/mmcblk0p2 rootfstype=ext3 rootwait mem=128M mpurate=450 androidboot.console=ttyS2
once up, enable network with
netcfg eth0 dhcp
Hi all,
this issue is solved. See the tread
http://e2e.ti.com/support/embedded/android/f/509/p/160372/871858.aspx#871858
With best regards
Christian