Tool/software: Linux
Hi
I am using Linux Processor SDK 05.00.00.15v for Sitara AM5718.
1. I want to know does the LCD1 and LCD2 supports preoressive and interlaced video format respectively ?
2. In processor SDK Linux user guide's Kernel Driver part it is mentioned that omapdrm driver does not support for Interlace as LCD output.If so , can we achieve this any way by using 'scaler' which is a supported feature in DRM Plane Features ?
3. Does the LCDs support 1024*768 and 640*480 resolutions ?
(Also mentioned that On the EVM board, we use DPI LCD panel of resolution 800 x 480.)
Thanks and Regards
Arpita