Tool/software: Linux
Hi,
I'm building the processor sdk 05.00.00.15 in ubuntu 16.04. Due to the lack of sufficient HDD space, I have enabled INHERI
T
+= "rm_work"
in my conf/local.conf file. After running bitbake arago-core-tisdk-image I see some errors in do_configure state in some recipes (image-rotate, cv-camera, ar-track-alvar, image-proc, depth-image-proc). After reading the error log file, for example for the depth-image-proc case, I found this error:
...
CMake Error in CMakeLists.txt:
Imported target "opencv_xphoto" includes non-existent path
"/home/smart/Projects/arago-project/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/cv-bridge/1.11.16-r0/recipe-sysroot/usr/include/opencv"
...
It seems that there is an issue regarding cv-bridge package. I rebuilt this recipe, this time without INHERI
T
+= "rm_work"
. After that I could easily bake all those failing recipes.
Why do I have to do this? Is this a bug in the new processor sdk or I've missed something? If this is a known bug, is there any patch to resolve it?
Thank you.