This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VICP [DM6446]

Dear Experts,

                  I recently downloaded and installed the VICP library available at http://focus.ti.com/docs/toolsw/folders/print/sprc831.html

                  I opened a sample color conversion project and tried to run it. I see that in the linker options the following libraries are used

                  imx644x.lib;IP_run644x.lib;imgproc644x.lib;GPP_imgproc644x.lib;edma3_drv_bios.lib;edma3_rm_bios.lib;dmcsl644x_bios.lib.

                 Are these libraries installed along with the VICP as I get linker error when I tried to build the project.

-Rgds

Vallabha