Team,
Regarding using GPMC for NAND:
I assume that it is possible to use multiple NAND devices on the GPMC.
-Are there some restriction on which GPMC_CSNx should be used when multiple NAND need to be used?
-Is there an ECC module present for every CSN memory space? or is there one single ECC module for the entire GPMC?
-Are the SW drivers (Linux, RTOS) supporting multiple NAND devices interfaced on the GPMC?
Thanks in advance,
Anthony