This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L2 Banking Scheme Implemented on DM6446



Hi, all:

1.  What's the banking scheme implemented of the level two memory on DM6446?

    4 x 128-bit banks, or 2 x 128-bit banks, or 1 x 256-bit banks?

2.  Is the level two memory of DM6446 work on 198 MHz with 594 MHz core?

 

thanks a lot!