This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: SATA termination calibration

Part Number: AM5728

On customer board SATA Rx signal level less than 270mV which is SATA standard required, From SATA standard, there is termination Calibration should can be used to adjust it. but not find it in TRM. Does AM57xx SATA support Termination Calibration? and how to use?

BTW, TX signal is OK.

  • Hi Tony,
    SATA termination calibration to 100 Ohms differential is performed as part of final test. There is no user control of this value.

    As PCB layout can have a significant impact on the channel impedance, please have the customer review SPRAAR7 looking for deviations from the layout recommendations contained therein.