Part Number: AM5728
Tool/software: TI-RTOS
I used External Camera Sensor API to drive ar0132 at TI-RTOS project. But there were some wrong when debug into Fvid2_create function, the whole initial function is pasted bellow:
int cr_vin2a_initial_bsp(Fvid2_Handle *fvid2handle)
{
// Typicall API calling sequence for video decoder in context of video capture application would be like below
//
// Fvid2_create() - create the sensor driver instance and take the sensor to standby
// IOCTL_BSP_VID_SENSOR_GET_CHIP_ID - check if device is active
// IOCTL_BSP_VID_SENSOR_GET_FEATURES - To get the sensor information and support
// IOCTL_BSP_VID_SENSOR_SET_CONFIG - setup the device for a particular mode
// Fvid2_start() - Start sensor
// Fvid2_stop() - Take sensor to standby
// Fvid2_delete() - delete sensor driver device
// Delete the capture driver
Bsp_VidSensorCreateParams crtParams;
Bsp_VidSensorCreateStatus crtStatus;
Bsp_VidSensorChipIdStatus chipidStatus;
Bsp_VidSensorConfigParams cfgParams;
crtParams.deviceI2cAddr[0] = 0x10;
crtParams.deviceI2cInstId = 4;//IC5
crtParams.deviceResetGpio[0] = BSP_VID_SENSOR_GPIO_NONE;
crtParams.numDevicesAtPort = 1;
crtParams.numSensorCfg = 1;
crtParams.sensorCfg = &crtParamsCfgReg;
crtParamsCfgReg.regAddr = 0x3140;
crtParamsCfgReg.regMask = 0xFFFF;
crtParamsCfgReg.regValue = 0x0001;
chipidStatus.chipRevision = 0;
chipidStatus.firmwareVersion = 0;
0,
&crtParams,
&crtStatus,
NULL);
fvid2handle = &fvid2Handle;
chipidParams.deviceNum = 1;
Fvid2_control( fvid2Handle,
IOCTL_BSP_VID_SENSOR_GET_CHIP_ID,
&chipidParams,
&chipidStatus);
IOCTL_BSP_VID_SENSOR_GET_FEATURES,
&features,
NULL);
cfgParams.bpp = FVID2_BPP_BITS12;
cfgParams.dataformat = FVID2_DF_RAW12;
cfgParams.fps = FVID2_FPS_5;
cfgParams.height = 720;
cfgParams.width = 1280;
cfgParams.standard = FVID2_STD_AUTO_DETECT;
cfgParams.videoIfWidth = FVID2_VIFW_12BIT;
IOCTL_BSP_VID_SENSOR_SET_CONFIG,
&cfgParams,
NULL);
}
Could anyone help me to find the mistakes?
I know there are some examples in pdk,but it's pretty complex cause so many stream and channels are used in the example. But I just want to drive only AR0132(mono mode) in my project.