Other Parts Discussed in Thread: OMAP-L137
I want to run program from External NOR flash. So how can i program the external nor flash using TMS320C6747 without JTAG Interface.
Is there any documents and articles related too.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to run program from External NOR flash. So how can i program the external nor flash using TMS320C6747 without JTAG Interface.
Is there any documents and articles related too.
I have OMAP-L137(EVM)
I done programming through Serial port(UART2) arranged boot switches as below.
Pin# | 7 | 2 | 1 | 0 | 3 |
Position | ON | OFF | ON | OFF | OFF |
Using Serial Boot and Flash Loading Utility ,but after reset the board it was not running program from SPI flash,i have followed below procedure.
1)First i have loaded dsp-spi-ais.bin ,ubl-spi.bin and u-boot.bin from command prompt using this commands
D:\OMAP-L137_FlashAndBootUtils_2_40\OMAP-L137_FlashAndBootUtils_2_40\OMAP-L137\GNU>sfh_OMAP-L137.exe -flash_noubl -p COM5 dsp-spi-ais.bin
D:\OMAP-L137_FlashAndBootUtils_2_40\OMAP-L137_FlashAndBootUtils_2_40\OMAP-L137\GNU>sfh_OMAP-L137.exe -flash_noubl -p COM5 ubl-spi.bin
D:\OMAP-L137_FlashAndBootUtils_2_40\OMAP-L137_FlashAndBootUtils_2_40\OMAP-L137\GNU>sfh_OMAP-L137.exe -flash_noubl -p COM5 u-boot.bin
Successfully loaded.
2)In the next step using the same above command instead of bin file loaded my application.out file
this is also successfully loaded
3)Then i changed my boot switches to SPIBOOT0.
Pin# | 7 | 2 | 1 | 0 | 3 |
Position | OFF | ON | OFF | ON | OFF |
and reboot my board.
But it is not going to run my application from SPI flash,Can you suggest me where it is wrong.