Hello,
We have new boards with the new OMAPl137 rev 2.0. The hardware is exactly the same but the revision of the OMAP L137 is different ( before we had rev 1.0 ) We are loading the same firmware ( dspais, armubl, u-boot and linux ) on the rev 1.0 and rev 2.0 but none of our 2.0 boards boot correctly.
Sometimes it hangs before u-boot sometimes after...
Our boards boots from NAND. We use the same flash writer. It seems to flash correctly the dspais , arm ubl and u-boot as it verifies the data after. We use the original dspais comming with in the PSP DaVinci-PSP-SDK-03.20.00.12, and the same ubl. ( our ubl just modifies the PIN MUX )
Our first board hangs before u-boot:
Booting with TI UBL
Device OPP (300MHz, 1.2V)NAND Boot failed.
BOOTUBLBOOTUBLBOOTUBLBOOTUBLBOOTUBLBOOTUBLBOOTUBLBOOTUBLBOOTUBL
The second during uboot
Booting with TI UBL
Device OPP (300MHz, 1.2V)
U-Boot 2009.11 (Nov 01 2010 - 15:34:05)
Board: BRUTUS
Proceeding to normal boot sequence...
I2C: ready
DRAM:
and it hangs here....
We have seen that the dsp ROM code has changed in the new revision but we use the standard precompiled dsp-ais.bin found in the PSP. Is there anything we must modify ?
Thanks for your help.
Jeremy