This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: AM5708 reference design questions

Part Number: AM5708

What would be the best reference design to follow for the AM5708?
I see reference designs for the AM571x and AM572x, but none for the AM570x series.

Is there a similar compatibility guide that includes the AM570x series?
http://www.ti.com/lit/an/sprabx8e/sprabx8e. pdf 

Thanks
RD

  • RD,

    Please refer to the AM570x 6-Layer PCB Reference Design at .

    SPRABX8 is a compatibility guide between AM572x, AM574x and AM571x since these devices are pin-compatible under the implementation constraints provided.  They are all available in the same 23mm package.  AM570x is available in a 17mm reduced-cost package and is not pin-compatible with any other device in the AM57xx family.  It is electrically same as the AM571x for the pins available in the AM570x.  This detail is available in the DM and the TRM.

    Tom