Part Number: AM3352
Hi,
We currently have AM3352BZCZD80 on our BOM. Out software team are concerned about the speed not being 1GHz
800MHz Cortex A8, silicon Rev 2.1 in 324BGA (ZCZ, 0.8mm pitch) package, -40°C to +90°C
If we desire a 1GHz version what options do we have ?
AM3352BZCZ100 1000MHz Cortex A8, silicon Rev 2.1 in 324BGA (ZCZ, 0.8mm pitch) package, 0°C to +90°C
Can we use the AM3352BZCZ100 at 600MHz below 0°C
Can we use the AM3352BZCZD80 at 1000MHz between 20°C and 55°C ?
Thanks,
Jani