This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BEAGLEBN: BBONEGRNW

Part Number: BEAGLEBN

Tool/software: Linux

I have made several unsuccessful attempts to activate SPI1 (config-pin 9.28 spi_cs for example) on a Beaglebone Green Wireless(BBGW). My implementation of the most recent solution suggested by RoberCNelson on his response to a similar issue(link below) causes the wireless feature of my BBGW to stop working. Then I need to re-load the image to the eMMC because I am unable to reestablish connection to the BBGW.

I am able to configure and access SPI0 without any problems.

I will appreciate any additional suggestions to solve this issue.

 https://groups.google.com/forum/embed/?place=forum/beagleboard&showsearch=true&showpopout=true&showtabs=false&hideforumtitle=true&parenturl=https%3A%2F%2Fbeagleboard.org%2Fdiscuss#!searchin/beagleboard/P9_28/beagleboard/RShjePl0noY/uwryVY8MBwAJ 

Thanks

Luis Mendez

 

My system setup is as follows:

root@beaglebone:/# cat etc/debian_version

9.5

 root@beaglebone:/# sudo /opt/scripts/tools/version.sh

git:/opt/scripts/:[1aa73453b2c980b75e31e83dab7dd8b6696f10c7]

eeprom:[A335BNLTGW1ABBGW16055109]

model:[TI_AM335x_BeagleBone_Green_Wireless]

dogtag:[BeagleBoard.org Debian Image 2018-06-17]

bootloader:[eMMC-(default)]:[/dev/mmcblk1]:[U-Boot 2018.03-00002-gac9cce7c6a]:[location: dd MBR]

kernel:[4.14.71-ti-r78]

nodejs:[v6.14.4]

uboot_overlay_options:[enable_uboot_overlays=1]

uboot_overlay_options:[disable_uboot_overlay_video=1]

uboot_overlay_options:[disable_uboot_overlay_audio=1]

uboot_overlay_options:[enable_uboot_cape_universal=1]

pkg check: to individually upgrade run: [sudo apt install --only-upgrade <pkg>]

pkg:[bb-cape-overlays]:[4.4.20180928.0-0rcnee0~stretch+20180928]

pkg:[bb-wl18xx-firmware]:[1.20180517-0rcnee0~stretch+20180517]

pkg:[kmod]:[23-2rcnee1~stretch+20171005]

pkg:[roboticscape]:[0.4.4-git20180608.0-0rcnee0~stretch+20180609]:[GOT_REPLACED_BY_NEXT]

WARNING:pkg:[librobotcontrol]:[NOT_INSTALLED]

pkg:[firmware-ti-connectivity]:[20170823-1rcnee1~stretch+20180328]

groups:[debian : debian adm kmem dialout cdrom floppy audio dip video plugdev users systemd-journal i2c bluetooth netdev cloud9ide gpio pwm eqep admin spi tisdk weston-launch xenomai]

cmdline:[console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 quiet]

dmesg | grep pinctrl-single

[    1.076672] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568

dmesg | grep gpio-of-helper

[    1.088000] gpio-of-helper ocp:cape-universal: ready

END

root@beaglebone:/# ls -al /dev/spidev*

crw-rw---- 1 root spi 153, 0 Oct  1 21:46 /dev/spidev1.0

crw-rw---- 1 root spi 153, 1 Oct  1 21:46 /dev/spidev1.1

crw-rw---- 1 root spi 153, 2 Oct  1 21:46 /dev/spidev2.0

crw-rw---- 1 root spi 153, 3 Oct  1 21:46 /dev/spidev2.1

 

root@beaglebone:/# config-pin -q 9.28

P9_28 pinmux file not found!

Cannot read pinmux file: /sys/devices/platform/ocp/ocp*P9_28_pinmux/state

 

root@beaglebone:/sys/devices/platform/ocp# ls

40300000.ocmcram  48044000.timer     481ae000.gpio    53500000.aes          ocp:P8_30_pinmux  ocp:P8_44_pinmux  ocp:P9_23_pinmux

44e07000.gpio     48046000.timer     481cc000.can     driver_override       ocp:P8_31_pinmux  ocp:P8_45_pinmux  ocp:P9_24_pinmux

44e09000.serial   48048000.timer     481d0000.can     modalias              ocp:P8_32_pinmux  ocp:P8_46_pinmux  ocp:P9_25_pinmux

44e0b000.i2c      4804a000.timer     481d8000.mmc     ocp:cape-universal    ocp:P8_33_pinmux  ocp:P9_11_pinmux  ocp:P9_26_pinmux

44e0d000.tscadc   4804c000.gpio      48300000.epwmss  ocp:l4_wkup@44c00000  ocp:P8_34_pinmux  ocp:P9_13_pinmux  ocp:P9_27_pinmux

44e35000.wdt      48060000.mmc       48302000.epwmss  ocp:P8_07_pinmux      ocp:P8_35_pinmux  ocp:P9_14_pinmux  ocp:P9_41_pinmux

44e3e000.rtc      480c8000.mailbox   48304000.epwmss  ocp:P8_08_pinmux      ocp:P8_36_pinmux  ocp:P9_15_pinmux  ocp:P9_42_pinmux

47400000.usb      480ca000.spinlock  48310000.rng     ocp:P8_09_pinmux      ocp:P8_37_pinmux  ocp:P9_16_pinmux  ocp:P9_91_pinmux

47810000.mmc      4819c000.i2c       49000000.edma    ocp:P8_10_pinmux      ocp:P8_38_pinmux  ocp:P9_17_pinmux  ocp:P9_92_pinmux

48022000.serial   481a0000.spi       49800000.tptc    ocp:P8_13_pinmux      ocp:P8_39_pinmux  ocp:P9_18_pinmux  of_node

48024000.serial   481a6000.serial    49900000.tptc    ocp:P8_19_pinmux      ocp:P8_40_pinmux  ocp:P9_19_pinmux  power

4802a000.i2c      481a8000.serial    49a00000.tptc    ocp:P8_27_pinmux      ocp:P8_41_pinmux  ocp:P9_20_pinmux  subsystem

48030000.spi      481aa000.serial    4c000000.emif    ocp:P8_28_pinmux      ocp:P8_42_pinmux  ocp:P9_21_pinmux  uevent

48042000.timer    481ac000.gpio      53100000.sham    ocp:P8_29_pinmux      ocp:P8_43_pinmux  ocp:P9_22_pinmux