This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Qt-Gstreamer integration issue

Part Number: PROCESSOR-SDK-AM335X


Tool/software: Linux

Hello,

I am using ti-processor-sdk-linux-am335x-evm-04.01.00.06 SDK and beaglebone black bsp based custom board.

I am using ti-toolchain for compiling Qt/QML code.but in this tool chain QtGstreamer tool chain is not present.

To compile and integrate the QtGstreamer module in tool chain i downloaded source  git://anongit.freedesktop.org/gstreamer/qt-gstreamer

and i followed below steps to compile it

1. cd  linux-devkit

2. source environment-setup

3. cd qt-gstreamer

4. mkdir build && cd build

5. cmake  -DCMAKE_INSTALL_PREFIX=/usr -DQT_VERSION=5 -DQTGSTREAMER_STATIC=ON -DQTGSTREAMER_EXAMPLES=OFF -DQTGSTREAMER_CODEGEN=OFF

but not able to configure  it and make file did not create.

I tried another method.

1. i install boost

2. I tried t reconfigure qt-gstreamer but did not get success.

Errors:

/usr/include/python2.7/pyconfig.h:24:54: fatal error: arm-linux-gnueabihf/python2.7/pyconfig.h: No such file or directory
 #  include <arm-linux-gnueabihf/python2.7/pyconfig.h>
                                                      ^
compilation terminated.

-- Performing Test USE_OPENGLES - Failed
-- Could NOT find OpenGL (missing:  OPENGL_gl_LIBRARY OPENGL_INCLUDE_DIR)
CMake Error at cmake/modules/FindQt4or5.cmake:203 (qt5_use_modules):
  Unknown CMake command "qt5_use_modules".
Call Stack (most recent call first):
  src/QGlib/CMakeLists.txt:53 (qt4or5_use_modules)


-- Configuring incomplete, errors occurred!
See also "/home/rahul/Rahul/PROJECTS/HMain/H-Main-Linux-kernel/Qt_support/qt-gstreamer-1.2.0/1.2.0/qt-gstreamer-1.2.0/build/CMakeFiles/CMakeOutput.log".
See also "/home/rahul/Rahul/PROJECTS/HMain/H-Main-Linux-kernel/Qt_support/qt-gstreamer-1.2.0/1.2.0/qt-gstreamer-1.2.0/build/CMakeFiles/CMakeError.log".
make: *** No targets specified and no makefile found.  Stop.
rm: missing operand
Try 'rm --help' for more information.
rm: missing operand
Try 'rm --help' for more information.

can you please suggest me how can i proceed to install qt-gstreamer in ti-toolchain and rfs.