Other Parts Discussed in Thread: TVP5146
I have interfaced cmos sensor MT9D13 with DM6437 and used the example program modified with decoder TVP5146. I have connect CDDC[0..7], VD, HD, PXCLK and these signals seem to be good. I have also set 3.3 V to TVP5146_ENABLE to disable bus switch. Cmos sensor is set with I2C routine different from that used in the example. When program arrives to FVID_EXCHANGE, it remain blocked. I have also tried to repeat the same code with TVP5146 decoder, with TVP5146_ENABLE set and using TVP5146 signalconnected directly on the DC_P1, but it doesn't work. If I remove 3.3V from TVP5146_ENABLE pin the decoder works, but I can't use obviously CMOS sensor. What I do wrong?
Thanks,
David