This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TNETV107X : Cannot find tnetv107x_evm_config

Hello,

I try to compile u-boot to load into the tnetv107x platoform. I follow the instructions posted here :

Unfortunately, I cannot compile and because the config file is not present

***
*** Can't find default configuration "arch/../configs/tnetv107x_evm_defconfig"!
***
scripts/kconfig/Makefile:114: recipe for target 'tnetv107x_evm_defconfig' failed
make[1]: *** [tnetv107x_evm_defconfig] Error 1
Makefile:477: recipe for target 'tnetv107x_evm_config' failed
make: *** [tnetv107x_evm_config] Error 2

Please could you indidcate where I can find the good repo with the config file and corresponding sources for the TNETV107X ?

kind regards

sk