This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3: Processor SDK Radar AppImage didn't work

Part Number: TDA3
Other Parts Discussed in Thread: AWR1243

Hi,

I have an TDA3 RVP and xWR1242 radar module from D3 Engineering. I am using the Processor SDK Radar to build an AppImage for the platform based on the instruction provided in the Radar SDK UserGuide. I specifically set the configuration to tda3xx_rvp_bios_radar in the Rules.make config file to build the AppImage. The AppImage size turned out to be about 5.8MB. I then copied the AppImage to the SD that comes with the D3 firmware and replaced the existing AppImage on the card. Inserted the card into the RVP and boot it up. I also have the tera terminal console connected from the RVP to the PC. This worked with the firmware comes with the SD card from D3. However, the AppImage I built from the Radar SDK didn't work at all. There is no console output to Tera Terminal on my PC.

However, when I built the AppImage using the tda3xx_evm_bios_radar, it's simi-working. There is console output on Tera Terminal for this AppImage. However, when I tried to exercise to the Radar use cases, I got I2C errors in log below. Please help resolving this issue.

Thanks,

--Khai

[IPU1-1] 1.926066 s: ***** IPU1_1 Firmware build time 13:51:00 Oct 4 2018
[IPU1-1] 1.926218 s: *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
[IPU1-1] 1.926615 s: SYSTEM: System Common Init in progress !!!
[IPU1-1] 1.927286 s: SYSTEM: IPC init in progress !!!
[IPU1-1] 1.927377 s: SYSTEM: IPCLIB init in progress !!!
[IPU1-1] 1.927652 s: SYSTEM: IPCLIB: register to [IPU1-0] event 15...
[IPU1-1] 1.927743 s: SYSTEM: IPCLIB: register to [DSP1] event 15...
[IPU1-1] 1.927835 s: SYSTEM: IPCLIB: register to [EVE1] event 15...
[IPU1-1] 1.927896 s: SYSTEM: IPCLIB init DONE !!!
[IPU1-1] 1.927957 s: SYSTEM: Notify init done !!!
[IPU1-1] 1.928140 s: SYSTEM: MsgQ init done !!!
[IPU1-1] 1.928353 s: SYSTEM: Work Queue init done !!!
[IPU1-1] 1.928414 s: SYSTEM: IPC init DONE !!!
[IPU1-1] 1.930549 s: SYSTEM: System Common Init Done !!!
[IPU1-1] 1.930641 s: SYSTEM: System IPU1_1 Init in progress !!!
[IPU1-1] 1.931373 s: UTILS: DMA: HWI Create for INT25 !!!
[IPU1-1] 1.931525 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
[IPU1-1] 1.931647 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261960 B (255 KB)
[IPU1-1] 1.931830 s: SYSTEM: Initializing Links !!!
[IPU1-1] 1.974867 s: UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
[IPU1-1] 1.976331 s: UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
[IPU1-1] 1.977947 s: UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
[IPU1-1] 1.979442 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
[IPU1-1] 1.981058 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
[IPU1-1] 1.982706 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
[IPU1-1] 1.984322 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
[IPU1-1] 1.986091 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
[IPU1-1] 1.987830 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
[IPU1-1] 1.989507 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
[IPU1-1] 1.991398 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
[IPU1-1] 1.991520 s: SYSTEM: Initializing Links ... DONE !!!
[IPU1-1] 1.991581 s: SYSTEM: System IPU1_1 Init Done !!!
[DSP1 ] 2.044195 s: SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
[DSP1 ] 2.044226 s: SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
[EVE1 ] 1.970200 s: SYSTEM: Initializing Links ... DONE !!!
[EVE1 ] 1.970963 s: SYSTEM: System EVE Init Done !!!
[IPU1-0] 3.076648 s: QSPI Init Started
[IPU1-0] 3.076862 s: MID - 20
[IPU1-0] 3.076923 s: DID - ba
[IPU1-0] 3.076953 s: QSPI Init Completed Sucessfully
[IPU1-0] 3.079698 s: UTILS: DMM: API NOT supported in TDA3xx !!!
[IPU1-0] 3.079790 s: UTILS: DMM: API NOT supported in TDA3xx !!!
[IPU1-0] 3.080339 s:
[IPU1-0] 3.080400 s: Current System Settings,
[IPU1-0] 3.080461 s: ========================
[IPU1-0] 3.080491 s: Display Type : HDMI 1920x1080 @ 60fps
[IPU1-0] 3.080583 s: My IP address : none
[IPU1-0] 3.080613 s:
[IPU1-0] 3.080705 s: ============
[IPU1-0] 3.080735 s: Usecase Menu
[IPU1-0] 3.080796 s: ============
[IPU1-0] 3.080827 s:
[IPU1-0]
[IPU1-0] Vision SDK Usecases,
[IPU1-0] --------------------
[IPU1-0]
[IPU1-0] 1: RADAR Usecases
[IPU1-0] 2: MISC Tests
[IPU1-0]
[IPU1-0] s: System Settings
[IPU1-0]
[IPU1-0] x: Exit
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 10.097206 s:
[IPU1-0] 10.097328 s:
[IPU1-0]
[IPU1-0] RADAR Usecases
[IPU1-0] ---------------
[IPU1-0]
[IPU1-0] 2: Radar (Single AWR1243) Capture + Null (TDA3xx Only)
[IPU1-0] 3: Radar (Single AWR1243) Capture + Radar Object Detect (EVE1) + Display (TDA3xx Only)
[IPU1-0] 4: Radar (Single AWR1243) Capture + Radar Object Detect (EVE1) + Null (TDA3xx Only)
[IPU1-0] 5: Radar (Single AWR1243) Capture + Radar Frame Copy (DSP1) + Null (TDA3xx Only)
[IPU1-0]
[IPU1-0] x: Exit
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 19.033154 s:
[IPU1-0] 19.033306 s: CHAINS: Init AR12xx ...
[IPU1-0] 19.033550 s: UTILS_MCSPI: McSPI is configured in interrupt mode!!
[IPU1-0] 19.034008 s: src/bsp_deviceI2c.c @ Line 667:
[IPU1-0] 19.034160 s: I2C0: DEV 0x20: ERROR !!!
[IPU1-0] 19.034221 s: src/bsp_deviceI2c.c @ Line 689:
[IPU1-0] 19.034313 s: I2C0: Error timeout 0 ms!!!
[IPU1-0] 19.034404 s: src/bsp_boardTda3xx.c @ Line 2535:
[IPU1-0] 19.034465 s: I2C write failed!!
[IPU1-0] 19.034831 s: src/bsp_deviceI2c.c @ Line 667:
[IPU1-0] 19.034892 s: I2C0: DEV 0x20: ERROR !!!
[IPU1-0] 19.034984 s: src/bsp_deviceI2c.c @ Line 689:
[IPU1-0] 19.035075 s: I2C0: Error timeout 1 ms!!!
[IPU1-0] 19.035289 s: src/bsp_boardTda3xx.c @ Line 2545:
[IPU1-0] 19.035350 s: I2C write failed!!
[IPU1-0] 19.035716 s: src/bsp_deviceI2c.c @ Line 667:
[IPU1-0] 19.035807 s: I2C0: DEV 0x23: ERROR !!!
[IPU1-0] 19.035899 s: src/bsp_deviceI2c.c @ Line 689:
[IPU1-0] 19.035960 s: I2C0: Error timeout 1 ms!!!
[IPU1-0] 19.036051 s: src/bsp_boardTda3xx.c @ Line 1961:
[IPU1-0] 19.036143 s: I2C read failed!!
[IPU1-0] 19.036204 s: src/bsp_board.c @ Line 620:
[IPU1-0] 19.036265 s: Device select failed!!

  • Hi Khai,

    Which version of Processor SDK Radar are you using?

    Thanks and Regards,
    Piyali
  • Khai,

    tda3xx_evm_bios_radar is not the right config for the RVP board. I am following up with the team to confirm if they are able to reproduce the issue you are facing with respect to the boot of the app image.

    Thanks and Regards,
    Piyali
  • Hi Piyali,

    Thanks for looking into the problem.

    The AppIMage built for tda3xx_evm_bios_radar at least runs and shows the console output with some I2C error when tried to run a use case. The tda3xx_rvp_bios_radar AppImage didn't show anything on the console.

    Regards,

    --Khai

  • Hi Khai,

    I don't see any issue with tda3xx_rvp_bios_radar AppImage from Radar SDK 3.5 on RVP. There are 2 com ports which will show up after connecting USB cable to RVP.
    Did you select the second one?

    Regards,
    Stanley
  • Hi Stanley,

    When I run using the second serial port for console output, this is what I got:


    Ú0`b$U
    @D(¢ @ü
    TDA3xx SBL Boot

    Identified 15X15 Silicon

    DPLL Configuration Completed

    Clock Domain Configuration Completed

    Module Enable Configuration Completed

    TI EVM PAD Configuration Completed

    DDR Configuration Completed

    TDA3xx SOC Init Completed

    App Image Download Begins

    SD Boot - file open completed successfully

    IPU1 CPU0 Image Load Completed

    IPU1 CPU1 Image Load Completed

    DSP1 Image Load Completed

    EVE1 Image Load Completed

    App Image Download Completed

    EVE MMU configuration completed

    *****************************************************************

    32K Timer is used to measure cycles, divide by 32K to get time in seconds

    Reset to SBL Init Cycles - 10436 (318.48 ms)

    SBL Initial Config Cycles - 332 (10.13 ms)

    SOC Init Cycles - 493 (15.04 ms)

    DDR Config Clock Cycles - 230 (7.01 ms)

    App Image Load Cycles - 49958 (1524.59 ms)

    Slave Core Bootup Cycles - 709 (21.63 ms)

    SBL Boot-up Cycles - 51723 (1578.46 ms)

    *****************************************************************

    Jumping to IPU1 CPU1 App

    Jumping to IPU1 CPU0 App
    [IPU1-0] 1.951320 s: ***** IPU1_0 Firmware build time 09:43:41 Oct 5 2018
    [IPU1-0] 1.951503 s: *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
    [IPU1-0] 1.951808 s: SYSTEM: System Common Init in progress !!!
    [IPU1-0] 1.959647 s: SYSTEM: IPC init in progress !!!
    [IPU1-0] 1.959738 s: SYSTEM: IPCLIB init in progress !!!
    [IPU1-0] 1.960043 s: SYSTEM: IPCLIB: register to [IPU1-1] event 15...
    [IPU1-0] 1.960165 s: SYSTEM: IPCLIB: register to [DSP1] event 15...
    [IPU1-0] 1.960257 s: SYSTEM: IPCLIB: register to [EVE1] event 15...
    [IPU1-0] 1.960348 s: SYSTEM: IPCLIB init DONE !!!
    [IPU1-0] 1.960409 s: SYSTEM: Notify init done !!!
    [IPU1-0] 1.960623 s: SYSTEM: MsgQ init done !!!
    [IPU1-0] 1.960958 s: SYSTEM: Work Queue init done !!!
    [IPU1-0] 1.961080 s: SYSTEM: IPC init DONE !!!
    [IPU1-0] 1.963185 s: SYSTEM: System Common Init Done !!!
    [IPU1-0] 1.963277 s: SYSTEM: System Init in progress !!!
    [IPU1-0] 1.963338 s: SYSTEM: BSP Common Init in progress !!!
    [IPU1-0] 1.963399 s: SYSTEM: BSP Common Init Done !!!
    [IPU1-0] 1.963460 s: SYSTEM: BSP Platform Init in progress !!!
    [IPU1-0] 1.963582 s: SYSTEM: BSP Platform Init Done !!!
    [IPU1-0] 1.963643 s: SYSTEM: FVID2 Init in progress !!!
    [IPU1-0] 1.963765 s: SYSTEM: FVID2 Init Done !!!
    [IPU1-0] 1.963826 s: SYSTEM: VPS Init in progress !!!
    [IPU1-0] 1.963887 s: SYSTEM: VPDMA Descriptor Memory Address translation ENABLED [0xa0000000 -> 0x80000000]
    [IPU1-0] 1.966357 s: *** VPDMA Firmware Loading... ***
    [IPU1-0] 1.966479 s: VPDMA Firmware Address = 0x9ffc7800
    [IPU1-0] 1.966540 s: VPDMA Load Address = 0x4897d004
    [IPU1-0] 1.966662 s: VPDMA Firmware Version = 0x4d0001b8
    [IPU1-0] 1.966723 s: VPDMA List Busy Status = 0x00000000
    [IPU1-0] 1.966815 s: *** VPDMA Firmware Load Success ***
    [IPU1-0] 2.000213 s: SYSTEM: VPS Init Done !!!
    [IPU1-0] 2.001006 s: UTILS: DMA: HWI Create for INT34 !!!
    [IPU1-0] 2.001311 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [IPU1-0] 2.001403 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261568 B (255 KB)
    [IPU1-0] 2.001586 s: SYSTEM: Heap = SR_OCMC @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
    [IPU1-0] 2.001738 s: SYSTEM: Heap = SR_DDR_CACHED @ 0x85703000, Total size = 369086464 B (351 MB), Free size = 369086464 B (351 MB)
    [IPU1-0] 2.001921 s: SYSTEM: Heap = SR_DDR_NON_CACHED @ 0x00000000, Total size = 0 B (0 MB), Free size = 0 B (0 MB)
    [IPU1-0] 2.002104 s: SYSTEM: Initializing Links !!!
    [IPU1-0] 2.078234 s: SYSTEM: Initializing Links ... DONE !!!
    [IPU1-0] 2.094552 s: BOARD: Board Init in progress !!!
    [IPU1-0] 2.095010 s: BOARD: Board Init Done !!!
    [IPU1-0] 2.099280 s: RVP Late Init
    [IPU1-0] 2.099341 s:
    [IPU1-0] 2.099402 s: Vision SDK Version : [REL_VISION_SDK_03_05_00_00]
    [IPU1-0] 2.099463 s: FVID2 Version : [FVID_02_01_00_01]
    [IPU1-0] 2.099524 s: BSP Version : [PDK_01_10_01_xx]
    [IPU1-0] 2.099585 s: Platform : [EVM]
    [IPU1-0] 2.099646 s: SOC : [TDA3XX]
    [IPU1-0] 2.099707 s: SOC Revision : [ES2.0]
    [IPU1-0] 2.099768 s: Board Detected : [TDA3XX RVP A]
    [IPU1-0] 2.100012 s: Base Board Revision : [REV A 2G]
    [IPU1-0] 2.100073 s: Daughter Card Revision: [REV A]
    [IPU1-0] 2.100134 s:
    [IPU1-1] 1.958427 s: ***** IPU1_1 Firmware build time 09:42:15 Oct 5 2018
    [IPU1-1] 1.958579 s: *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>
    [IPU1-1] 1.960104 s: UTILS: DMA: HWI Create for INT25 !!!
    [IPU1-1] 1.988013 s: SYSTEM: System Common Init in progress !!!
    [IPU1-1] 1.988318 s: SYSTEM: IPC init in progress !!!
    [IPU1-1] 1.988440 s: SYSTEM: IPCLIB init in progress !!!
    [IPU1-1] 1.988653 s: SYSTEM: IPCLIB: register to [IPU1-0] event 15...
    [IPU1-1] 1.988775 s: SYSTEM: IPCLIB: register to [DSP1] event 15...
    [IPU1-1] 1.988867 s: SYSTEM: IPCLIB: register to [EVE1] event 15...
    [IPU1-1] 1.988958 s: SYSTEM: IPCLIB init DONE !!!
    [IPU1-1] 1.989080 s: SYSTEM: Notify init done !!!
    [IPU1-1] 1.989324 s: SYSTEM: MsgQ init done !!!
    [IPU1-1] 1.989660 s: SYSTEM: Work Queue init done !!!
    [IPU1-1] 1.989751 s: SYSTEM: IPC init DONE !!!
    [IPU1-1] 1.992069 s: SYSTEM: System Common Init Done !!!
    [IPU1-1] 1.992161 s: SYSTEM: System IPU1_1 Init in progress !!!
    [IPU1-1] 1.992222 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [IPU1-1] 1.992344 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 236352 B (230 KB)
    [IPU1-1] 1.992527 s: SYSTEM: Initializing Links !!!
    [IPU1-1] 2.034953 s: UTILS: PRF: ##### Cannot allocate Object for SYNC1 ####
    [IPU1-1] 2.036570 s: UTILS: PRF: ##### Cannot allocate Object for SYNC2 ####
    [IPU1-1] 2.038156 s: UTILS: PRF: ##### Cannot allocate Object for SYNC3 ####
    [IPU1-1] 2.039681 s: UTILS: PRF: ##### Cannot allocate Object for TFDTPRX ####
    [IPU1-1] 2.041511 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM0 ####
    [IPU1-1] 2.043463 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM1 ####
    [IPU1-1] 2.045476 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM2 ####
    [IPU1-1] 2.047520 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM3 ####
    [IPU1-1] 2.049594 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM4 ####
    [IPU1-1] 2.051881 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM5 ####
    [IPU1-1] 2.054077 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM6 ####
    [IPU1-1] 2.056365 s: UTILS: PRF: ##### Cannot allocate Object for ALGORITHM7 ####
    [IPU1-1] 2.056487 s: SYSTEM: Initializing Links ... DONE !!!
    [IPU1-1] 2.056792 s: SYSTEM: System IPU1_1 Init Done !!!
    [IPU1-1] 2.259256 s: NSP GMAC: PHY 12 Found on MAC Port 0
    [DSP1 ] 2.084426 s: SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
    [DSP1 ] 2.084456 s: SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
    [EVE1 ] 1.999359 s: SYSTEM: Initializing Links ... DONE !!!
    [EVE1 ] 2.000091 s: SYSTEM: System EVE Init Done !!!
    [IPU1-0] 3.101018 s: QSPI Init Started
    [IPU1-0] 3.101201 s: MID - 20
    [IPU1-0] 3.101232 s: DID - ba
    [IPU1-0] 3.101293 s: QSPI Init Completed Sucessfully
    [IPU1-0] 3.104068 s: UTILS: DMM: API NOT supported in TDA3xx !!!
    [IPU1-0] 3.104190 s: UTILS: DMM: API NOT supported in TDA3xx !!!
    [IPU1-0] 3.105075 s:
    [IPU1-0] 3.105136 s: Current System Settings,
    [IPU1-0] 3.105197 s: ========================
    [IPU1-0] 3.105258 s: Display Type : HDMI 1920x1080 @ 60fps
    [IPU1-0] 3.105319 s: My IP address : 0.0.0.0
    [IPU1-0] 3.105349 s:
    [IPU1-0] 3.105380 s: ============
    [IPU1-0] 3.105441 s: Usecase Menu
    [IPU1-0] 3.105471 s: ============
    [IPU1-0] 3.105532 s:
    [IPU1-0]
    [IPU1-0] Vision SDK Usecases,
    [IPU1-0] --------------------
    [IPU1-0]
    [IPU1-0] 1: RADAR Usecases
    [IPU1-0] 2: MISC Tests
    [IPU1-0]
    [IPU1-0] s: System Settings
    [IPU1-0]
    [IPU1-0] x: Exit
    [IPU1-0]
    [IPU1-0] Enter Choice:
    [IPU1-0]
    [IPU1-1] 7.056121 s: NETWORK_CTRL: Starting Server (port=5000) !!!
    [IPU1-1] 7.056365 s: NETWORK_CTRL: Starting Server ... DONE (port=5000) !!!
    [IPU1-0] 11.733087 s:
    [IPU1-0] 11.733209 s:
    [IPU1-0]
    [IPU1-0] RADAR Usecases
    [IPU1-0] ---------------
    [IPU1-0]
    [IPU1-0] 3: Radar (Single AWR1243) Capture + Radar Object Detect (EVE1) + Display (TDA3xx Only)
    [IPU1-0] 7: Multi Radar (AWR1243) Capture + Radar FFT (EVE1) + Display (TDA3xx Only)
    [IPU1-0]
    [IPU1-0] x: Exit
    [IPU1-0]
    [IPU1-0] Enter Choice:
    [IPU1-0]
    [IPU1-0] 22.853413 s:
    [IPU1-0] 22.853474 s: Unsupported option '2'. Please try again
    [IPU1-0] 22.853809 s:
    [IPU1-0]
    [IPU1-0] RADAR Usecases
    [IPU1-0] ---------------
    [IPU1-0]
    [IPU1-0] 3: Radar (Single AWR1243) Capture + Radar Object Detect (EVE1) + Display (TDA3xx Only)
    [IPU1-0] 7: Multi Radar (AWR1243) Capture + Radar FFT (EVE1) + Display (TDA3xx Only)
    [IPU1-0]
    [IPU1-0] x: Exit
    [IPU1-0]
    [IPU1-0] Enter Choice:
    [IPU1-0]
    [IPU1-0] 24.485451 s:
    [IPU1-0] 24.485542 s:
    [IPU1-0]
    [IPU1-0] =======================
    [IPU1-0] Select Number of Radars
    [IPU1-0] =======================
    [IPU1-0]
    [IPU1-0] Enter Number of Radars are connected: (1-4)
    [IPU1-0]
    [IPU1-0] 26.212651 s: CHAINS: 1 AR12xx connected via FPD-Link...
    [IPU1-0] 26.212834 s:
    [IPU1-0]
    [IPU1-0] ========================
    [IPU1-0] Unit Test case Selection
    [IPU1-0] ========================
    [IPU1-0]
    [IPU1-0] 1: Default Sample Normal Frame Configuration
    [IPU1-0]
    [IPU1-0] 2: Default Sample Advanced Frame Configuration
    [IPU1-0]
    [IPU1-0] 3: Binary Phase Modulation
    [IPU1-0]
    [IPU1-0] 4: Finite Frames
    [IPU1-0]
    [IPU1-0] 5: Test Pattern Generation
    [IPU1-0]
    [IPU1-0] Enter Choice:
    [IPU1-0]
    [IPU1-0] 31.269017 s: CHAINS: Init AR12xx ...
    [IPU1-0] 31.269535 s:
    [IPU1-0]
    [IPU1-0] ==========================
    [IPU1-0] Select UB960 Configuration
    [IPU1-0] ==========================
    [IPU1-0]
    [IPU1-0] 1: 2Gbps Mode
    [IPU1-0] 2: 4Gbps Mode
    [IPU1-0]
    [IPU1-0] Enter Choice:
    [IPU1-0]
    [IPU1-0] 32.653510 s: CHAINS: UB960 is configured for 2Gbps Mode
    [IPU1-0] 32.653602 s: Using AR12xx
    [IPU1-0] 32.653663 s: src/bsputils_ub960.c @ Line 1962:
    [IPU1-0] 32.653724 s: Failed to detect board ID
    [IPU1-0] 33.453028 s: Detected 964 v3 DeSerializer
    [IPU1-0] 40.906057 s: Port 0 done
    [IPU1-0] 41.033062 s: AR12XX: ES2.0 Device detected!!
    [IPU1-0] 41.119105 s: AWR12XX: Version Master : 1.9.0.7
    [IPU1-0] 41.119227 s: AWR12XX: Version RF:1.9.1.7
    [IPU1-0] 41.119319 s: AWR12XX: Version mmWaveLink:1.2.0.0
    [IPU1-0] 41.119410 s: AWR12XX: Version Master Patch[dd.mm.yy]:78.224.4
    [IPU1-0] 41.119502 s: AWR12XX: Version RF Patch[dd.mm.yy]:0.0.0
    [IPU1-0] 41.162050 s: Assertion @ Line: 273 in C:/TI/PROCESSOR_SDK_RADAR_03_05_00_00/vision_sdk/apps/src/rtos/radar/src/common/chains_common_ar12xx.c: SYSTEM_LINK_STATUS_SOK == retVal : failed !!!

  • Hi Khai,

    After fixing the break statement in e2e.ti.com/.../735990, are you able to proceed without assertion or you are still facing an assertion with this fix?

    Thanks and Regards,
    Piyali
  • No, still get the assertion at line 273 of chains_common_ar12xx.c

    While building the VSDK code after fixing the break statement, I saw this error during build:

    C:/TI/PROCESSOR_SDK_VISION_03_04_00_00/vision_sdk/apps/configs/autorules_footer_cfg.mk:78: ipc_PATH does not exist! (). Is this OK or that can be a problem?
  • I also noticed while building, I got these warnings, not sure if they are OK:

    "C:/TI/PROCESSOR_SDK_VISION_03_04_00_00/vision_sdk/links_fw/src/rtos/bios_app_common/tda3xx/cfg/link_eve.cmd", line 12: warning: no matching section "C:/TI/PROCESSOR_SDK_VISION_03_04_00_00/vision_sdk/links_fw/src/rtos/bios_app_common/tda3xx/cfg/link_eve.cmd", line 13: warning: no matching section "C:/TI/PROCESSOR_SDK_VISION_03_04_00_00/vision_sdk/links_fw/src/rtos/bios_app_common/tda3xx/cfg/link_eve.cmd", line 18: warning: no matching section
  • BTW, I am switching to building the Vision SDK. I see no difference between the two.
  • So the assertion because the retval is SYSTEM_LINK_STATUS_EALLOC and not SYSTEM_LINK_STATUS_SOK
  • Hi Khai,

    The problem you are seeing is the firmware compatibility on the D3 radar module.

    Radar SDK 3.5 require AWR12XX: Version Master: 1.10.0.23.

    [IPU1-0] 41.033062 s: AR12XX: ES2.0 Device detected!!
    [IPU1-0] 41.119105 s: AWR12XX: Version Master : 1.9.0.7
    [IPU1-0] 41.119227 s: AWR12XX: Version RF:1.9.1.7
    [IPU1-0] 41.119319 s: AWR12XX: Version mmWaveLink:1.2.0.0

    Could you contact D3 to find out how to get your module firmware to update to 1.10?

    Otherwise, you have to use Radar SDK 3.1 release @ http://software-dl.ti.com/processor-sdk-vision/esd/TDAx/radar-sdk/03_01_00_00/index_FDS.html

    Regards,

    Stanley