Hi,
Is there any example available for review for UnderRun/OverRun USB Error handling in C55x5 ?
Christos
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is there any example available for review for UnderRun/OverRun USB Error handling in C55x5 ?
Christos
Hi Christos,
We do not have UnderRun/OverRun USB error handling example code in C5515. If you are using Bulk or Interrupt modes than you may do the tests using the current CSL USB example program along with the Host side application.
If you are using the ISO mode, I can send you a simple CSL based ISO test program. You can use it to develop your own test program.
Best regards,
Ming