This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2E: emmc boot issue

Expert 1615 points

Part Number: TDA2E

Hi,

Recently, when we run tda2eg,

there is an error when the system startup on emmc(mmc2_2) ,

there is a partition table error,

I can see that the mmc2 write speed can only support 48MHZ in the extra file of tda2x,

trace code finds dra72x Is running in HS200 mode,

so we try to reduce the frequency of HS200 to 52MHZ,

and finally solve this problem,

does the boot problem of mmc2 in tda2x also exist in tda2eg?

Use visionsdk3.02

smallJ