Other Parts Discussed in Thread: RFSDK, DAC38J84, ADC14X250
Tool/software: TI C/C++ Compiler
,how is DFE in " DFE BYPASS MODE"? Is there a DFE BYPASS example?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
There is an infrastructure for controlling the internal DMA structure from DDR3 memory to IQNet buffers to DFE, to JESD, to Serdes and the Rx is the reverse order.
The infrastructure is called RFSDK, " http://www.ti.com/tool/rfsdk "
Within the RFSDK concept there is a 66AK2L06, ADC14x250, DAC38J84, and DLC card that are part of a TI design. " tidub89 "
This is the closest released configuration to DFE bypass
Tx is not DFE bypassed
input 122.88e6 -> DDUCTx PFIR filter, Resampler 3/2 184.32, CFR is effectively bypassed, CDFR Resample 4/3, DPD and Tx Frequency translates to 61.44 transmitted at 245.76Msps Tx,
on the Rx side 245.76Msps real,
Lane0 takes the I data from DAC IQ,the Rx performs Hilbert transform 61.44 -> 0, 122.88Msps complex, the Rx passes the 122.88msps to the Rx DDUC.
The Rx DDUC PFIR filters.
Please setup to use this configuration.
Regards,
Joe Quintal