Tool/software: Linux
Goodmorning,
I'm using a beaglebone balck and I have succesfully created the arago-rootfs.tisdk-image and meta-toolchain-arago-tisdk.
In conf/local.conf I added DISTRO_FEATURES_remove = " wayland" since I wanted to use EGFLS mode only. Unfortunately I get the following error:
EGLFS: Failed to open /dev/fb0
EGLFS: Can't continue without a display
I can confirm you that there is no /dev/fb0 fle, however on hdmi monitor I can see the Arago prompt for logging in.
How can I add /dev/fbo? Besides if I wanted to have an external LVDS display as /dev/fb1, is it sufficient to add its dts file in the board device tree?
Thank you in advance.