This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dose the DM365 IPNC support frame buffer display?



Hi everyone,

         We need use frame buffer as display device. When I add the frame buffer support in the kernel, then I can find the device files /dev/fb/[0, 1, 2, 3]. But when I use dev/fb/3 to display, I can't get the image on the TV out. And if I use the /dev/video2 to display, I will get a opened error: 

 ERROR  (drv_display.c|DRV_displayOpen|138): open device /dev/video2

 ERROR  (drv_capture.c|DRV_captureTestOpen|338): Open failed

          Could anybody help me?

 

Thanks,

Yanbin Yue