This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the Problem TSIF on DM6467



Hello all:

    Who has tested the TSIF on DM6467?  The TSIF interface is on  DC_P2 connector  on DM6467 , I  want to test the parallel,synchronous,and input model of TSIF0,

    I haved designed a TSIF connector in order to connect the TSIF interface on DC_P2 to another board(a board has the function as TS analyzer),and there only eleven pins:

1.TS0_CLKIN(TSIF0 receive clock input )

2.TS0_EN_WAITO(date enable)

3.TS0_PSTIN(packet start)

4.TSDIN0——TSDIN7(data)

The above is my hardware,and I install the TSIF driver,compile the application (saTsifUserPtrBuffer and so on),and I use oscilloscope to measure the above eleven pins,all normal,so The TSIF source is right,it can produce the right TS signal.But when I execute the application:

./ ./saTsifUserPtrBuffer 60000 60000 60000 60000 ,it only turn out only the followings information:

-------------------Send the Data from the MPEG2 TS Analyzer

Last,I put some debug information in the TS Driver,I found it can't  execute the irqreturn_t tsif_isr(int irq, void *dev_id, struct pt_regs *regs) function, so  it can't produce interrupt.

 The application I have changed some, although I only configure it BYPASS model to receive any packets ,still can't produce interrupt.

  Anyone encounter the above question? If some problem is related to  my HardWare ?but I think the parallel,synchronous,and input model of TSIF0 only 11 pins,am I right?

   Thanks everyone!