This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: TMDXIDK571 and configuration support

Part Number: AM5718

Tool/software: Linux

Field came with following question:

Does our TMDXIDK571 running Linux RT supports the following configuration?

Ethernet (2xPRU + 2x Gib) + LCD + PRU-ICSS IND SW (PRP/HSR/IEC61xxx) at the same time.

  • Hi Rogerio,

    To answer this question there is some more information needed and experimentation required. With RT there a system latency target the developer will have in mind and require their target to meet that is within acceptable statistical limits. The system latency will vary based on the use-case. So the above use-case could be configured but I would recommend experimenting to find if the above configuration will meet the target requirements for latency.

    Best Regards,
    Schuyler
  • Schuyler,

    Thanks for the response. I have sent this link to the field and in case there are more questions, they will post here.