Dear All,
I am a newbie to TMS320DM642. I got TMS320DM642 EVM (Spectrum Digital) from my company.
My problem is how I can communicate with the EVM as it was connected to my PCI slot. I am not using any JTAG emulators.
When I am trying with CC Studio, it is reporting that the EVM has not been powered up.
I installed the PCI drivers from Spectrum digital and the Switches (S1 and S2) are made in such a way that the board operates with HPI/PCI boot using default PCI registers.
Can I download my code to EVM using CCS through PCI? Or is there any other compiler which can build and download the code to EVM through PCI without using any JTAG?
Thanks in advance,
Regards,
Ramya