Part Number: AM5718
Other Parts Discussed in Thread: DM3725
Tool/software: Linux
Hi all,
Can anyone please help me in resolving following queries,
1. As per the response to the supported Output format and Linux driver of LCD (Interlace/Progressive) output, "Interlace feature has DSS IP level limitation for LCD but for HDMI, it’s driver level limitation."
But in the TRM document(SPRUHZ7G), multiple times its mentioned that "Configurable LCD output mode: progressive or interlace mode"(Page No. 2667-LCD Outputs) and "The LCD output can be configured in progressive output or interlace output. The selection is done by writing into the DISPC_CONFIGo[22] OUTPUTMODEENABLE bit.(Page No. 2744). Can anyone please clarify my doubt that is it possible to get interlaced output at any of the LCD outputs(LCD1/2/3) or the TV Output ??
2. If we can get then how ?? And can we achieve this by modifying/writing any Linux driver for Interlace output ?
3. The following is mentioned in page no. 2693(DISPC Progressive-to-Interlaced Format Conversion).
"The DMA engine can be used to perform YUV4:2:0 NV12 and YUV4:2:0 NV21 progressive-to-interlaced
data conversion with 0-degree orientation. Such conversion performed in the DSS consists of separating
each progressive frame into two fields containing odd and even lines.This section provides generic
approach details."
What does it mean exactly and is it useful to get Interlace output anyway ? If so, how ?
4. Does any of the TI processors have the Interlace output supported Linux driver for LCD/TV ? (Is the source code available)
5. As per the below DSS guide, in "Unsupported Features/Limitations" chapter,
software-dl.ti.com/.../Foundational_Components_Kernel_Drivers.html
AM57xx processor supports for Progressive Driver for LCD/TV.
Where can I get that perticular driver (which directory in the Linux SDK ) ?
NOTE : I am Using AM5718 based custom board and Linux Processor SDK version 05.00.00.15.
Any help is appreciated .
Thanks and regards...
Arpita Jena