This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: TMS320C6748EZWTA3

Part Number: TMS320C6748

Hi,

 

What's the difference between TMS320C6748BZWT3 (obsolete) and TMS320C6748EZWTA3 (can this be used as an "drop in" alternative) ?

 

  

 

Best regards

Niklas

  • Hi Niklas,

    The chip designation is explained in the Datasheet in Section 7.1 Device Nomenclature.

    Best Regards,
    Yordan
  • Niklas,

    Here is clarification of TMS320C6748BZWT3 nomenclature:
    B = Revision 2.0
    ZWT = PACKAGE TYPE 361-Pin Plastic BGA, with Pb-free Soldered Balls [Green], 0.8-mm Ball Pitch
    Blank = 0°C to 90°C, Commercial Grade
    3 = 375 MHz (Revision 2.x)
    and TMS320C6748EZWTA3:
    E = Revision 2.3
    ZWT = PACKAGE TYPE 361-Pin Plastic BGA, with Pb-free Soldered Balls [Green], 0.8-mm Ball Pitch
    A = –40°C to 105°C, Extended Grade
    3 = 375 MHz (Revision 2.x)

    BR
    Tsvetolin Shulev