Other Parts Discussed in Thread: OMAPL138
Tool/software: TI-RTOS
Hi All,
I am using pdk_omapl138_1_0_6 for LCDKOMAPL138.
I have two devices over same SPI bus (bus 1). Configuration for both the devices are different, one is in 4-pin mode and another one is in 3-pin. I tried configuring and using them at the same time and it was failing. On looking inside the spi driver it seems that at a time I can open one handle for one bus with one chip select. Meaning I cannot use both the devices at the same time.
So, is this pdk driver drawback or hardware issue?
Thanks...