This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808EVM linux uncompression error

Other Parts Discussed in Thread: AM1808, OMAPL138

Hi,

I am using AM1808 EVM and try to rebuild the kernel and boot from the NFS. I am refering the following url for the same

http://processors.wiki.ti.com/index.php/GSG:_Building_Software_Components_for_OMAP-L1#Rebuilding_the_Linux_kernel

Compiled the kernel in the following way. The kernel source is from the DVD, that comes with AM1808 EVM ( Linux-2.6.33-rc4)

        make distclean
        make da850_omapl138_defconfig
        make uImage modules
        make INSTALL_MOD_PATH=$(ROOTFS) modules_install

Also build busybox and populate NFS properly.

My bootargs is


setenv bootcmd 'tftp c2000000 uImage';setenv autostart yes;setenv bootargs 'console=ttyS2,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.161.15:/rootfs ,nolock mem=32M';

On booting I got the following error

 

## Booting kernel from Legacy Image at c2000000 ...
   Image Name:   Linux-2.6.33-rc4
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2126892 Bytes =  2 MB
   Load Address: c0008000
   Entry Point:  c0008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux...

uncompression error

Any help will be appreciated.

--Batsayan