Part Number: AM5748
HI,
I am presently working on Sitara AM5748 Processor.
I am presently doing pin multiplexing in mux_data.h file which is a part of U-Boot source.
Once the kernel is loaded will the pin multiplexing done from U-Boot source will be over written?
If so where am I supposed to configure the pin multiplexing in kernel source?
I am using SDK version "ti-processor-sdk-linux-am57xx-evm-05.00.00.15-Linux".
Thanks ,
Janardan M