Hi,
1. Working on the DM6446, I have customized the driver to allow the number of buffers allocated in the driver configurable through a command line argument. However, for counts above 4, I find that the allocation fails. I have a 256MB board and use 62MB for linux pool. I think 5 buffers of 720x605x2 bytes size should be allocatable in the present configuration. Can anyone comment?
2. The total memory on the board is shared by the linux pool and the codec engine space. Does allocating extra memory in the CMEM space vis-a-vis increasing the driver buffers has any trade-off in terms of DSP system performance?
Thanx!
Sundar