Other Parts Discussed in Thread: AM3703, AM3505, DM3725, AM3517
Hello,
I am trying to compare the power consumption between the OMAP3 3505 and OMAP3 3725 by using appropriate Power Estimation Spreadsheet.
- 3505 is running at 25C@600MHz , SDMA&SDRC - Estimated max, USB - Isochronous, all other N/A.
VDD_CORE=272mW / Peripheral’s = 66mW / PLL's +Iq=148.99mW => The power tally full VDD_CORE is 487.44mW (Table D)!!!!
Total IC power ~ 815mW
When the same conditions are used for the power consumption estimation OMAP3 3725 , the power tally full VDD1 & VDD2 are 260+60=320mW (Table D)!!!!
The total IC power ~ 529mW !!!!!
Please clarify the differences of ~300mW?
Thanks
Vitaliy