This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA3XEVM: TDA3xEVM running vps_test_display failed

Part Number: TDA3XEVM

Tool/software: TI-RTOS

I build PDK 

The binary is in C:\PROCESSOR_SDK_VISION_03_02_00_00\ti_components\drivers\pdk_01_08_01_06\packages\ti\binary

Then I running the vps_test_display

1. load the file to TDA3x IPU1_0 (vps_test_display_ipu1_0_debug.xem4)

2. then the error happened

Cortex_M4_IPU1_C0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)

How Can I fix it???