This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Davinci EVM Reset Circuitry

The Davinci EVM reset circuitry is designed to pull the output of U46 & U45 low in the event of DSP_CORE_VDD dropping out. However, the reset signal (1.8V.SYS_RESETz) to the DM6446 coming from U44 will not cause the processor's reset to be pulled low, due to diode D5. If DSP_CORE_VDD is lost shouldn't the processor reset (1.8V.SYS_RESETz) also be pulled low to reset the processor in the event that DSP_CORE_VDD comes back up?

 

Regards,

Eric