This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Can I trust memory bandwidth of omapconf ?

Part Number: AM5728


Tool/software: Linux

Hi.

I execute omapconf for real memory bandwidth.

our board doesn't attach usb.but, memory bandwidth display wrong value(1841.66)

omapconf trace bw --tr0 r --m0 usb1

root@am57xx-evm:~# omapconf trace bw --tr0 r --m0 usb1 
OMAPCONF (rev v1.73 built Wed Jun 28 18:45:28 EDT 2017)

HW Platform:
  Generic DRA74X (Flattened Device Tree)
  DRA75X ES2.0 GP Device (STANDARD performance (1.0GHz))
  TPS659038  ES2.2

SW Build Details:
  Build:
    Version:  _____                    _____           _         _  
  Kernel:
    Version: 4.9.28-geed43d1050
    Author: jhlee@ubunto-TI
    Toolchain: gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11)
    Type: #2 SMP PREEMPT
    Date: Thu Oct 18 14:49:24 KST 2018

Counter: 0  Master:            usb1 Transaction:  r Probe: emif1
Counter: 1  Master:          alldmm Transaction:  w Probe: emif2
Counter: 2  Master:          alldmm Transaction:  r Probe: emif1
Counter: 3  Master:          alldmm Transaction:  r Probe: emif2
delay in us: 1000000
overflow delay in us: 1000000 (iterations=1)
accumulation type: 2
iterations (0=infinite): 0
Overflow counter index: DISABLED (overflow delay used)
Overflow threshold: DISABLED (overflow delay used)
              Time Stamp(32KHz ticks) ->   Throughput(MB/s)
time:         End       Start   Delta ->   Counter0   Counter1   Counter2   Counter3
time:   579449319   579416518   32801 ->    1841.66    1780.40    1841.66    1780.40
time:   579482111   579449319   32792 ->    1836.79    1776.56    1836.79    1776.56

we test other device for omapconf  (omapconf trace bw --tr0 r --m0 usb4 , omapconf trace bw --tr0 r --m0 vip1_p1, omapconf trace bw --tr0 r --m0 pcie_ss1, ....)

result is wrong value.

Can I trust memory bandwidth of omapconf ?

Thanks a lot.