I'm looking for an example of L137 EMIF-A module. Would appreciate if anybody would like to share. Prefer to be a CSLr code. Thanks a lot ! - Sean
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm looking for an example of L137 EMIF-A module. Would appreciate if anybody would like to share. Prefer to be a CSLr code. Thanks a lot ! - Sean
Can you elaborate more on the example needed? If you are using the OMAP-L137 EVM, the GEL file initializes and setup the EMIFA controller. After wards, you can access the EMIFA memory by performing normal reads and writes to the EMIFA MMR region.
If you need an example on how to read/write to the EMIFA memory after GEL initialization, please download the test code here, http://support.spectrumdigital.com/boards/evmomapl137/revg/. Under dsp\tests\sdram, modify the code to read from EMIFA memory instead of DDR.
--Christina