Hello all
I m using DM648 on my customized board with NDK 2 and running the Hello World Application. I am unable to send LAN packets greater than 1514 bytes. And if i send packet having 1514 byte length the packet is sent but CCS generates warning that EMAC_sendPacket( ) returned error 32000038. Is there any way to increase the LAN packet size in NDK 2 without enabling Jumbo Packets?
Also tell me that i have to load my code twice to run the application in ist attempt CCS halts at Hello World Application TC/IP Stack MAC Address **-**-**-** kindly tell the solution
Regards
Depp