Tool/software: Linux
Dear Sirs, We are having some trouble with USB1 interface of AM5718 used as HOST in HS mode (Only USB2.0 D+/D- signals are connectes). Randomly, the USB key connected to the port disconnects during a read or write operation. The conditions are:
1) The used USB Key is Data Traveler da 16GByte (see picture)
2) The linux Kernel is 4.9.45-rt23
More than one key of the same brand and model have been tested and all of them show the problem. The USB Key is a USB SS type key. Other two SS USB Key brands have been tested without any problem.
Have you had experience on this type of problem?
Thanks in advance